Controlled Stop

In a controlled stop, drive motion is brought to a standstill in a controlled manner. The drive commands a zero velocity from the motor. The motor decelerates at the prescribed deceleration value (AXIS#.CS.DEC ).

A controlled stop can occur in a number of ways:

  • The user configures a programmable Action (see Configuring Actions) to perform a Controlled Stop
  • Either a controller or the user (through the WorkBench terminal window) initiates a software disable (AXIS#.DIS ) command .
  • A fault initiates a controlled stop from the drive. See Faults and Messages for the faults which initiate a controlled stop.

An implicit controlled stop is also part of some other features which stop motion:

  • A fault occurs which has a controlled stop (CS) reaction. After the CS is executed, the drive disables.
  • HW limit switch: A digital input is defined as a positive or negative limit switch (AXIS#.HWLS.NEGSOURCE or AXIS#.HWLS.POSSOURCE). When the limit switch is met, the CS mechanism starts running. In this case, the parameter AXIS#.DISTO is not active.
  • SW limit switch: SWLS defines an active SW limit. When the limit is met, the CS mechanism starts running. In this case, the parameter AXIS#.DISTO is not active.

Use the drive CS parameters to configure a controlled stop as follows:

  1. AXIS#.CS.DEC : Deceleration ramp that is used for disable.
  2. AXIS#.DISVTHRESH: Velocity 0 threshold. The motor shaft is considered as stopped as soon as the actual velocity (filtered through a 10 Hz filter, such as AXIS#.VL.FBFILTER ) is within ± AXIS#.DISVTHRESH.
  3. AXIS#.DISTVTHRESH: Velocity 0 time. The actual velocity must be consecutively within 0 ± AXIS#.DISVTHRESH for the time AXIS#.DISTVTHRESHTO, before the drive completes the CS process. This value is used since the motor can overshoot out of the VEL0 window depending on the gains, deceleration ramp, motor inertia and so on.
  4. AXIS#.DISTO : Disable time out. This parameter sets an overall and independent running check as to whether or not the drive can achieve the disable state. If the VEL0 window set in step 3 is too small, it is possible that the drive may never reach the end of the CS process. The AXIS#.DISTO parameter and functionality addresses this issue by disabling the drive after the AXIS#.DISTO time elapses, even if the CS process did not end.

Controlled Stop Diagram

When configuring the controlled stop feature, please note the following:

The drive issues a fault F6005 in case that the AXIS#.DISTO counter expires during a controlled stop procedure.

Related Topics

CS Parameters

Configuring Actions

Faults and Messages

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen